Part Number: LMR36015-Q1 Tool/software: There are two packages listed in the data sheet for this device: ``RNX0012B'' and ``RNX0012C.'' Which is the "LMR36015FSC3RNXRQ1" package?
Part Number: LMR36015 Tool/software: Hello everyone,
I need to simulate the LMR36015 on a different simulator (SIMetrix) but it's engine it completely based on PSPICE, but when I add the .lib on this simulator and run the simulation it appear an error…
Part Number: LMR36015-Q1 Tool/software: I want to know the LMR36015-Q1 maximum transient voltage in ISO 7637-2 pulse 1&2a&3a&3b for a 24V system, as shown in other product figure below
Part Number: LMR36015 Tool/software: Hi,
This is regarding MPN - LMR36015FSCQRNXRQ1.
I captured the waveform of Inductor Current & Voltage across the switch.
My Doubt is:
1. I am seeing some weird behavior of Inductor Current while ramping up. As…
Part Number: LMR36015
Hi,
I want to use LMR36015ARNXR slightly differently as follows to get floating gnd. I did this to comeup with a cost efficient way of driving a Triac using a MCU powered by the Vout. The Triac MT1 is connected to AC_A. I am trying…
Part Number: LMR36015-Q1 Hi ,
This is regarding MPN - LMR36015FSCQRNXRQ1.
Can you please provide the current capability of Power Good (PG) Pin.
.Regards,
Ajay
Part Number: LMR36015-Q1 Hi ,
This is regarding MPN - LMR36015FSCQRNXRQ1. The .lib file available in the website is not working for Ansys tool.
Can you please provide me the common .lib file which will work for every tool.
& One more thing that while simulating…
Part Number: LMR36015-Q1 Hi TI expert,
May I know whether LMR36015-Q1 has any OVP mechanism?
I notice we do have current limit and minimum on-time requirement.
So if the OVP do happen on Vout side, the controller will only reduce the PWM & frequency until…
Part Number: LMR36015 Hi,
I have my design with LMR36015 quite advanced and I would like to have a feedback from TI.
Attached you will find a document with a description of the stack, sch, and layers.
There is a point, pin12 - SW node, where I would like…
Part Number: LMR36015-Q1 Hi ,
This is regarding MPN - LMR36015AQRNXRQ1 . I tried simulating the circuit with PSPICE Model for following data.
Input - 6V-36V
Output - 5V, 1A
Switching frequency - 400KHz
I got some issues that while simulating I am getting…