Part Number: LMZ14201H Tool/software: We're trying to settle an internal argument (and circuit) where we'd like to generate a -15 V rail from a +5 V rail using an LMZ14201H or similar IC. We are using the toplogy for an inverting buck-boost application…
Part Number: LMZ14201H Other Parts Discussed in Thread: LMZ14201 , , LMR36510 We currently have a design that uses an LMZ14201 to generate -5V.
System changes are driving us to need -12V or -15V instead.
Can we replace the LMZ14201 with an LMZ14201H, and…
Part Number: LMZ14201H Hi,
I simulate the LMZ14201H based circuit in Tina. I use Fig 8-1 design shown on datasheet.
Vout=5V, Vin=12V rise from 0V to 12V in 1ms, Rent=100k, Renb=17.3k
I got the LMZ14201H spice model from TI website, LMZ14201H Unencrypted…
Part Number: LMZ14201H Hi,
I´m trying to bould an adjustable power supplywith the LMZ14201H
Vin: 24V
Vout: adjustable from 5 to 22V (or whatever is maximum possible)
Iout: 3A
The idea is to realize Rfbb with a poti.
The question is how to choose…
Part Number: LMZ14201H Dear Team
Good day!
Our customer want to confirm some details of LMZ14201H.
When the LMZ14201H Vin is present, but the ENABLE pin is disabled, will the internal timer be switching? In other words, does the presence of Vin or the…
Part Number: LMZ14201H Hi,
I will use LM14201H in my project and I want to know is it operate when input voltage is lower than setted output voltage.
I want to get 12 V output at 40 V input applied but initialy I can supply 10 V and just 7-8 volt output…
Part Number: LMZ14201H Other Parts Discussed in Thread: LMZ14203H I need to develop a variable output power supply module capable of supplying a 5-24 volt output voltage at 5-1000mA. In experimenting with the LMZ14201H module in the WEBENCH tool, I struggled…
Part Number: LMZ14201H Hi Team,
A customer tried to simulate LMZ14201H with the following specifications, Vin =11V-14V, Vout=10V and Iout=0.5A. However, an error message below appeared in Webench. Is this a bug in Webench or because the difference between…
Part Number: LMZ14201H Other Parts Discussed in Thread: LMZ14203H , , LMZ14201 We use the LMZ1420xH series for many applications.
As already asked in the original thread, we experience EMI problems at 60-70MHz and 200MHz.
We tested different output capacitors…
Part Number: LMZ14201H Other Parts Discussed in Thread: LMZM23601 , LMZ34202 , TPA2005D1 , LMZ14201 Can the LMZ14201H be regulated down to 4.2V output ? The input voltage is 12V.