Hi Brijesh,
So I built a Processor Linux SDK using 8.05 with patches to U-Boot and the Linux Kernel and have the device booting to linux, it is currently still receiving the CRTC0 SYNC LOST message. I have attached my dmsg log to the bottom of the post…
Hi,
You can read the attached documents.
CC2530DK User Guide - SWRU208
CC2530-ZNP
CC2530 User Guide - SWRU191
CC2530 DKUG.pdf
CC2530ZNP Interface Specification.pdf
CC253x User Guide.pdf
Thanks,
PM
Joaquin,
When I tried creating a CCS project for the sample CSL I2C example for C6657, I realized that the code is made only for the following devices such as
SOC_TDA3XX, SOC_DRA78x, SOC_J721E, SOC_AM574x, SOC_AM572x, SOC_AM571x
and not for SOC_C6657…
Hello Chittapu,
Not sure what it is that you need from your image but you can learn more about the MMU APIs in the following Link:
https://software-dl.ti.com/processor-sdk-rtos/esd/AM65X/07_00_00_05/exports/docs/bios_6_82_01_19/docs/cdoc/index.html#ti…
Part Number: DRA746 Hi,
Customer and I use 6AO.1.0 prebuilt binary and VIS SDK 01.50.22.01 prebuilt binary but we’re not able to hear any Radio from Jacinto 6/Jacinto 6 Plus EVM with JAMR3.
We have read VIS user guide carefully and also took a look…
There are toolchain, compiler version infrmation in the CompilerTestCaseFiles.zip file.
CCS 11.2
ti-cgt-arm_20.2.7.LTS
Do you need to provide other information besides these?
thanks
7651.VCU_Model.pp.txt
4810.VCU_Model_data.pp.txt
Hi,
What is "TRM"?
If you are meaning data sheet I have, please see attached datasheet. it was downloaded when I was developing firmware.
msp430f6766.pdf
Best Regards,
Elly Lee
MSP430x6 Family User Guide.pdf
Hi victor,
Thanks for your detailed reply.
Hi Alson,
The PCI-e example in TI-RTOS SDK does support on EP(End point) mode. Please refer the following document,
from the PCI-e wiki document sprac59a.pdf
Kindly refer this documents also sprugs6d…
Part Number: MSP430F6779A
Hi TI support,
From data sheet, I have a question about LCDC setting
1) LCDCVCTL Register, What will happen if the instructions are not followed in red circle?
(slau208q-MSP430x5xx and MSP430x6xx Family User's Guide RevQ…
Hello,
The Linux SDK ( http://www.ti.com/tool/ti-15.4-stack-gateway-linux-sdk ) has the documentation for the CoP and its communication protocol. I've attached the document here so that you don't have to dig through the Linux SDK.
ti-15.4-stack…