I do not understand why you want that.
As far as I know, there is no errata for the following members yet.
MSP430F5500, MSP430F5501, MSP430F5502, MSP430F5503, MSP430F5504, MSP430F5505, MSP430F5506, MSP430F5507, MSP430F5508, MSP430F5509, MSP430F5510…
Hi zohar,
thanks for your reply.
I was comapring the two processors, and it tseems that the only differece is the number of GPIO, the package, and the number of USCIs (I2C/UART/LIN/IrDA/SPI)
http://focus.ti.com/paramsearch/docs/compareresults…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi Paul,
I use the MSP430 product selection page from https://www.ti.com/microcontrollers-mcus-processors/msp430-microcontrollers/products.html and save all parts in the spreadsheet. I use the filters to filter out parts. There are quite a few that…
Hi Akash,
The erase check and TX BSL version commands are members of the standard command set in BSLs V1.50 or higher but excluding 2.x BSLs. The MSP430G2544 is BSL Version 2.02, ergo no TX BSL version command support for this device.
You can go through…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use the…
msp430f5509.pdf Hello Ryan
Thank you for your replay. Attached is the datasheet. In page 21, The note describe that Applying a 1-MΩ resistor to ground is recommended. the question is that if not apply this resistor, what will happen?