Other Parts Discussed in Thread: MSP430FR6879 , MSP430FR6989 Hi Champs,
My customer has a metering related product using MSP430FR6879, RevC, and LPM3 was utilized. Some of FR6877 would be hanging or FRAM was changed. I have already suggested them to…
Part Number: MSP430FR6979 Other Parts Discussed in Thread: UNIFLASH , Hi experts,
My customer is using UniFlash to write to the MSP430FR6979 and is having problems.
OS: Win10
UniFlash: v6.4.0, v7.0.0
[1.Error when writing]: "Cannot read property…
Hi Daniel,
There are several that could potentially work (see attached excel), but the MSP430FR5962 seems to meet all the requirements, except it only has 8K RAM.
parametric-data.csv
There are signs that the following members are coming. Any hint when?
MSP430FR4131, MSP430FR4132, MSP430FR4133 MSP430FR5887, MSP430FR58871, MSP430FR5888, MSP430FR58881, MSP430FR5889, MSP430FR58891 MSP430FR5986, MSP430FR5987, MSP430FR59871, MSP430FR5988…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest software…
Hi Paul,
I use the MSP430 product selection page from https://www.ti.com/microcontrollers-mcus-processors/msp430-microcontrollers/products.html and save all parts in the spreadsheet. I use the filters to filter out parts. There are quite a few that…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use the…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave