Hello
I think it is best to prevent any back-feed from an external source into the regulator.
Please see the following application notes.
8640.slyt689_backfeed.pdf
3463.slvae57b.pdf
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest software…
Hi Paul,
I use the MSP430 product selection page from https://www.ti.com/microcontrollers-mcus-processors/msp430-microcontrollers/products.html and save all parts in the spreadsheet. I use the filters to filter out parts. There are quite a few that…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use the…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );
Which…