Part Number: OPA2171 Other Parts Discussed in Thread: OPA171-Q1 , OPA171 Hi,
I am using OPA2171AQ1 in my design.
In datasheet the common mode input voltage range(V.CM) is specified as (V-)-0.1 to (V+)-2 for typical temperature @25dC.
Need to know…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: OPA2171 , AMC1200 , UCC27424
Hi ,first thank you for reading my question.
This is problem I met:
L1 and N1 are the input AC voltage-220VAC.
I acquire the voltage…
Other Parts Discussed in Thread: OPA2171 , LM258 , OPA141 , OPA192 , OPA625 Hi.
Please refer to the attached screenshot of the simplified circuit. This is used in a DC application.
Notes:
1. The negative input is not necessarily at circuit ground…
Part Number: TLV4171 Other Parts Discussed in Thread: OPA2990 , TLV2171 , TLV9302 , OPA2171 , TINA-TI Hello, I'm trying to use TLV4171 in an inverting configuration to drive an LED. Following are my questions
1) Per datasheet, it says 25 mA is the ouput…
Other Parts Discussed in Thread: OPA2171 , OPA251 , OPA2251 , OPA227 , OPA277 , OPA244 , LM324 , TLV3702-Q1 , LMC6762 , TLV3702 I know this is long but please hang in there I need help on this please.
We are using the two op-amps in an OPA2171 as a…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…