Hi Arthur,
I apologize for the delay. Thank you for your patience.
I see where your confusion might be. It may be easier to think of the USB Hub as multiple ports rather than one. Each port (USB-C) would have a data role and a power role. The port connected…
Other Parts Discussed in Thread: DIT4096 , SRC4190 Hi,
I am designing a device which can transfers USB audio to AES-3 output by connecting PCM2707 and DIR4096 in their I2S features.
Since I want to limit the hardware components numbers, I selected hardware…
Hello everyone;
i want to make a project with PCM2707 bus powered but i need GND isolation from usb-pc ;
i was thinking to use DCR01 Miniature, 1W Isolated Regulated DC/DC Converter for isolation but i don't know if usb bus differential line is working…
Other Parts Discussed in Thread: PCM2704 Hello!
Can the PCM2704…PCM2707 ICs USB input signals be active applied from the USB PC port when the ICs are unpowered totally (Vbus=Vanalog=Vdd=0V)?
Will the PCM2704…PCM2707 ICs be fail-safe in this case…
Other Parts Discussed in Thread: PCM2706 , PCM2705 Hello! The PCM2706 (C), PCM2707(C) DAC ICs can control the USB host with the 7 commands like PLAY/PAUSE, Vol.+/-, NEXT TRACK, etc. What is necessary to control playing modes if the USB host is considered…
Other Parts Discussed in Thread: PCM2706 I have a circuit for the PCM2707 with the following schematic; http://imgur.com/Iie2wod It is meant to provide an I2S output, as well as featuring a headphone output. When connecting it to my PC (linux) it is recognised…
Other Parts Discussed in Thread: PCM2706C , PCM2706 , PCM2704C , PCM2705C , PCM2705 , PCM2704 , TUSB2036 Hello, I already read the PCM2707 (-C) datasheets, but the information given there is not fully clear. 1. Can I change the PCM2707 (2707C) IC S/PDIF output…
Part Number: PCM2707C Hi Experts,
Good day. Seeking advise on this query:
I want to use PCM2707 to convert usb to i2s. And then, I have to upsampling the i2s signal because the DAC that I want to use only allows 24bit 96kHz signal.
The problem is that…
Part Number: PCM2707C Hi Ti Team,
1,Is there any way to change the default name of the PCM2707 chip connected to the computer to the name we need, and solidify it inside the chip (that is, without i2C to control it)
2,The sound card of the computer cannot…
Hi,
We use PCM2707 in embed system, ARM core board( with wifi connection) USB --> PCM2707 --> I2S digital AMP --> speaker.
It download audio source from internet, and play. Now there is a problem that when playing m4a/aac format audio files,…