Part Number: PCM5102EVM-U Hello experts,
due to unavailability of supporter from Germany, I need help for further help.
please find attached file of detailed description.
RE PCM5102 IC - Discussion.msg
please help further to solve issue.
Regard, Moh…
Part Number: PCM5102EVM-U
Hello exprets,
I want to use 3-wire I2S with PCM5102EVM board.
I am giving power to board through USB cable and 3 signals are connected at right side (analoge side). I want to validate my connection because IC is not giving…
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5121 , PCM5100 Hi
We are now evaluate PCM5102EVM-U, our setup as below
1. remove all jumper from W3
2. I2S signal feed to W3 pin 20, 22, 24, and 26 with
SCK = 5.6MHz
BCK = 2.8MHz
LR clock…
Part Number: PCM5102EVM-U Hi team,
I'm trying to connect an external I2S source to PCM5102EVM-U. To do that I removed all the jumpers on W3.
Then connected jumpers as below.
FLT: GND(normal latency)
SCK: GND to use internal PLL
BCK: external source…
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5142 Hello,
I would like to ask you about EVM usage.
Is there any tool to generate input date to EVM?
If no tool, how to generate the data.
Thanks and best regards,
Katsu
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5142 , PUREPATHCONSOLE , PCM1862EVM , PCM5102A , PCM5102 , PCM1862 The Software I downloaded from the web (slac493a) is not for PCM5102EVM-U , but for: PCM5101EVM-S (see attached image) .
This version…
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5102 I'm trying to configure my PCM5102EVM to evaluate while using its optical or coaxial SPDIF inputs, but I don't own a Windows machine. The manual for the EVM is pretty vague, so…
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5102A , PCM5101A , Hi,
A customer measured audio performance of PCM5102EVM-U. The SNR was 106dB, so he made a complaint about it. Because it is worse 6dB than typical value of the PCM5102A specification…
Other Parts Discussed in Thread: PCM5102A , PCM5102EVM-U e2e,
We have a customer considering using the PCM5102A in a new design. They purchased a PCM5102EVM-U and need the User Guide for it. Is one available?
Thanks for your help.
Regards,
John Wiemeyer …