Part Number: PGA900 Hello,
We would like to ask about the internal polling rate of the PADC in the PGA900.
Looking through the datasheet and it seems to only mention the output I2C rate, but not how fast the PGA900 itself samples the analog signal at. …
Part Number: PGA900 Hello,
The manual for the PGA900 says that there is a test register (it is mentioned in both the I2C, SPI, and OWI sections). However, there is no other information regarding the register offset of said test register.
I would like…
Part Number: PGA900 Other Parts Discussed in Thread: TIDA-00851 ,
hello I am coding firmware using the TIDA-00851 board. I am contacting you because I have a problem with UART communication.
The version of CCS is 12.1.0.00007.
And the TIDA-00851 board and…
Hi Bob!
I am very grateful for your continued support.
I understood about OTP and DEVRAM. I want to run the code I wrote in the above thread even if I abandon the device. This is so that I can understand the process of programming the OTP. I plan to understand…
Part Number: PGA900 Other Parts Discussed in Thread: UNIFLASH We are trying to communicate with a PGA900 using I2C. I understand that if the microprocessor is running, the only registers available are the COMBUF registers. However, I cannot get the PGA900…
Part Number: PGA900 Hi
Q1. All PGA900 datasheets are in the form of a request to TI. Is there a limited number of sales partners?
Q2. Is it possible to get support for software etc. to develop the PGA900 on E2E?
Thanks,
Conor
Hi Bob,
thank you for your reply.
Good to know that it is basically possible. I think we will start with the evaluation board and have a test.
Best regards
Michael
Part Number: PGA900 Hello,
We are working on a PGA900 design and have a question regarding interfacing the internal registers.
in Table 12 “Control and Status Registers” there are DI page and DI offset. Our initial assumption is that the address…