Part Number: PMP10468 Hi,
I am not able to open the zip file for gerber files of the reference design.
Below error is noticed every time downloaded from TI website.
Kindly provide the gerber files for our layout reference.
Part Number: PMP10468 Hi Team,
Good day. I am posting this inquiry on behalf of our customer.
" For the reference design PMP10468, the input is 85VAC-264VAC, and the output is 24V 1A. I would like to implement this design in my system. However, the…
Hi,
PMP10276 is a design with 12V/2A output.
For both PMP10276 and PMP10468 design, I use mathcad calculation file I created by myself.
PMP10468RevA.mcd Mathcad - PMP10276RevA.pdf
Hope the files are useful.
Regards,
Sheng-Yang Yu
Hi Rajesh,
Thank you for reaching out.
The following is a 24V/1A reference which you could use for reference.
https://www.ti.com/tool/PMP10468
Rcs should be lower than the recommended value. Rlc and Rcs is advisible to follow as per datasheet as this…
Part Number: UCC28700 Other Parts Discussed in Thread: PMP10468 , , PMP Dears,
I have made AC/DC design refer to PMP10468, and now the output voltage fluctuates greatly, the schematic and waveform are as follows:
Please give some advice to improve it, thanks…
Part Number: PMP10468 Other Parts Discussed in Thread: PMP10276 , UCC28700 Hi,
i have tried to determine the resistor devider from the VS pin as in the design PMP10276 RevB. But i can´t get the values for the R4 = 75k.
As i follow the datasheet UCC28700…
Hello Derek,
Checking this transformer for 6.6V and 24V, total 5W, DC stacked outputs. what is your application?
750811647 not found on WE website. will check production status and similar OTS transformers tomorrow.
our application is 42 to 380VDC input…
Hi Jonathon,
You are correct, variant A is preferred. With variant B, the high-side, HV FET is always passing current. A 85VAC-265VAC QR or valley switching flyback is very common, low cost and fairly efficient. The valley switching reduces switching…
Other Parts Discussed in Thread: PMP10468 Hello Power Experts,
I'm looking for altium CAD and transformer data-sheet for 85VAC-264VAC Input, 24V 1A Output, PSR Flyback Reference Design, PMP10468.
Please provide me these, I need this to develop new reference…