Hi,
I got two questions about the reference design PMP10592.
What’s the actual load current? The internal reference for average current limiting is 50 mV and the current sense resistor is 50mΩ on the board PMP10592, so the load current should be 1 A…
Hi Martin,
This reference design presents LED driver design usign LM5175.
http://www.ti.com/tool/pmp10592?keyMatch=PMP10592&tisearch=Search-EN-Everything
regards
Part Number: LM5175-Q1 Other Parts Discussed in Thread: LM5175 Hi,
One of my customer is planning to use LM5175-Q1 in LED driver application. The specifications are as shown below.
Input: 8-18V,
Output: 1A Constant LED current with forward voltage around…