Hello Huang,
I would recommend the UCC28180 since it is a single-phase CCM controller. This controller can be used in your 1kW application, as shown below in page 1 of the UCC28180 datasheet. This will have the smallest size due to its high 250kHz max…
Part Number: PMP11062 Other Parts Discussed in Thread: UCC28722 Hello,
Reference design PMP11062.
I would like to run the 15v bias circuit from 160v B+ versus the 380 volt B+ in the existing circuit.
What values do I need to change in the existing 15v…
Hello Yunjing,
Please check out PMP11062 as a starting point. It is a reference design for a Universal AC Input, 380V/1kW CCM PFC using UCC28180.
Regards,
Sonal
Part Number: TIDA-01464 Other Parts Discussed in Thread: UCC28950 , UCC28019A , UCC28019 , UCC28180 , PMP11062 , PMP11211 , UCC256301 Dear Sir,
My customer would like design a 800W LED Driver power solution(I have TIDA-01464 reference design for 200W).
Spec…
Dear SHAHRIAR,
Thanks for interested in TI's solution.
For UCC28050, we have EVM on line you can purchase, but it only for 100W design.
www.ti.com/.../ucc28051evm
For UCC28070, we also have EVM on line, but it is for 300W design.
www.ti.com/...…
Other Parts Discussed in Thread: PMP11062 I'm looking for a PFC similar to the PMP11062 design, but packaging constraints meant that I'll likely have to use two chokes. Given this, it'd be nice if I could make it an interleaved design, but all the application…