Part Number: PMP4745 Hi E2E,
Our customer refer PMP4745 to design TPS23757.
But the MOS which customer use that had higher Qg lead to VGS can't pull low at the moment. (Please refer the waveform) (Customer MOS's Qg=42nC, PMP4745 MOS's Qg=17nC)…
Other Parts Discussed in Thread: TPS23753AEVM-004 Hello,
What will be the changes I need to make to the PMP4745 design if I want to replace the T3 (LAN magnetics) from the Gigabit version (H6062) to 10/100BASE version (HX2326NL)?
Thanks,
Yuval
Hi Kuber,
Wondering if you could provide some additional detail for this design, please. A block diagram and/or power tree would be very helpful in putting together some recommendations, as I want to be clear on what the exact requirements are before…
Hi MIchael,
We have PMP4745 which is 12V@1A application.
You can refere to application note, SLVA305C, to modify the schematic and match your spec.
--Ben
If this post answered your question, please click Verify Answer .