Part Number: UCC2897A Hi team..
We are using UCC2897A as below, VIN=24V, Vo= 5V/12A, schematic is the same as PMP5117. The switching frequency is 250kHz in customer application. When we do 8kV ESD contact to earth (have Y capacitor to board ground even…
Hi Ibran,
UCC2897A requires at least 13.2 V for start-up so please be sure your minimum input voltage is always >13.2 V to guarantee proper startup. You can search the TI reference design librar y but PMP5117 and PMP8366 are two examples of UCC2897A…
Part Number: UCC2897A Hi team,
My customer is using UCC2897A as below, VIN=24V, Vo= 5V/15A, schematic is the same as PMP5117. The switching frequency is 125kHz in customer application. When they do 8kV ESD contact to earth (have Y capacitor to board ground…
Lok
The best place to start is usually to search the database of available TI-Designs:
www.ti.com/.../refdesignsearchresults.tsp
Click on the "search power reference design parameters" button. Then you can search by input voltage range, output voltage…