Other Parts Discussed in Thread: PCM3070 , MSP430F2132 Hi all, we have designed a Soundbar, keeping RDK Value SB as reference. we have a problem with I2C communication happening between MSP430, EEPROM and PCM3070. .d43 file of processflow is successfully…
Other Parts Discussed in Thread: PCM3070 Hi all,
We have designed a Soundbar with RDK Value SB as reference, now this has to be integrated with CC8520-CC2590 module.
Pls share the procedure to configure (using Purepath wireless configurator) CC8520…
Other Parts Discussed in Thread: PCM3070 , CC8520 Hi all,
We have designed a Soundbar with RDK Value SB as reference, now this has to be integrated with CC8520-CC2590 module.
Pls share the procedure to configure (using Purepath wireless configurator…
Other Parts Discussed in Thread: CC8520 Hi,
I am integrating RDK Value SB to CC8520 to use wireless subwoofer. Do i need a pairing signal to be sent to cc8520 to start streaming. If it is the case some GPIOs are coming out of cc88520 connector. Can I use…
Other Parts Discussed in Thread: PCM3070 I am referring to RDK VALUE SB in my soundbar design. I have some doubts in software part.
We are loading the script generated from pure path into EEPROM on the board. At start up all the data from EEPROM is…
Hi Srinivas,
Regarding the DIR9001, what is the status on the following pins - VDD, VCC, CKSEL, ERROR, FMT1, FMT0, SOUT0, FSOUT1, /RST, SCKO, BCKO, LRCKO, DOUT?
Is the PCA9535 (IO expander) have the proper mapping between the output pin and the MSP430…
Other Parts Discussed in Thread: PCM3070 i am designing a soundbar referring to RDK Value SB. We assembled all components on PCB and then programming was done as explained in Ti Value SB Reference Design. we are able to program successfully. but the output…
Measuring actual voltages on VCx pin is the first thing I didand they are OK.
So far mystery is partly dispelled.
I temporarily put bq78350 to reset state and read registers from bq76930 directly (Thank God I placed test points on I2C line). That took a…
Other Parts Discussed in Thread: PCM3070 , TPA3123D2 , PCA9535 , PCM2705 Hi,
We have designed a Soundbar using RDK value SB as a reference. After successfully programming the PCM3070 and MSP430 the MSP430 is failing to boot up the PCM3070 which in turn we…
Hi all,
We have designed a Soundbar by keeping RDK Value SB as the reference. The design is working, but we are facing some problem, kindly any one help us regarding this issue.
Problem:
The design is basically for 24V-2A supply same as the reference…