Part Number: RF430F5978EVM I am trying to build and debug using the sample code for the RF4305978EVM. I am getting the Build warning #10204-D could not resolve index library "libmath.a" to a compatible version. Will this create a functional…
Part Number: RF430F5978EVM Hi,
I am currently using the RF430f5978 evaluation module and I am testing the MSP access instruction through the MRD2 reader.
The messages sent through the MRD are: 01 11 E8 A0 00 00 32 00 32 40 F3 00 11 22 33 44 99 9A 0A …
Part Number: RF430F5978EVM We received the EVM and tried to install the SW on a Win10 PC.
Everything went smooth, but running the demo does not detect any of the above devices !!
Checking in the device manager shows standard MS drivers installed ?!?
…
Part Number: RF430F5978EVM Hello.
I installed device drivers successfully by the procedure in the following answer.
* https://e2e.ti.com/support/wireless-connectivity/other-wireless/f/667/t/847227?tisearch=e2e-quicksearch&keymatch=RF430F5978EVM
However…
Part Number: RF430F5978EVM Hello,
Few questions about the evaluation kit:
What is the size of RF430F5978EVM only PCB?
Can we set the power level to reduce LF detection to ½ meter with the eval kit?
If not using a Windows PC, can the MRD2EVM and…
Part Number: RF430F5978EVM The user's guide for the RF430F5978 contains the following line in the introductions: "typically [the range is] ~ 2m with this set up, but it can reach up to 10m with an LF power transmitter". Does TI have an LF…
Part Number: RF430F5978EVM Hello,
I am attempting to pass a long address from the ID Tag from the MRD2 to the RF430F5978 using the Data after Wake feature described on pag. 771-3 in the SLAU378. When I attempt it, I cannot capture more than four additional…