Part Number: OPA827 Tool/software: Hello. I have a question about the document below. "slau522_TI Precision Designs Verified Design"
First Please check the error in the document below. 2.1 Detailed Schematic - 0.1Hz LPF(HPF) 2nd order G = 10 - 10Hz…
Part Number: AM6548
Hi Ti,
We are using Linux RT SDK 07.01.00.18 on our customized board.
And we found some gpio status not correct when boot into kernel for a while.
We configure GPIO1-49~52 as PRG0_PRU1_GPO0~3 and dts setting is as below…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: SK-TDA4VM , TDA4VM Tool/software: Hello All,
I've tried to boot QNX Image with SK-TDA4VM board and successfully boot the qnx image from QNX SDK 09_02_00_05. However, ethernet is not enabled and…
Hi RamPrasad,
PFA the dtb file we are using for this scenario....!! As .dtb file attachment was not happening, I have changes the extension of dtb to .txt. So could you please change the extension to .dtb when you try opening it..
Thanks & Regards…
Hi Zahid,
thanks for the hint.
But actually I would like to use the TI app as a starting point because it is tested with the reference design.
See e.g. page 16 for my idea of the app.
I quickly checked the specs for "HRP Heart Rate Profile" and…
Part Number: TMS320F28069M Hello,
We are working on a project that requires SCI bootloading for the F28069M. The customer has specified half duplex UART for the project.
Because we will be running out of SCI mode from the ROM code, we won't have direct…
Part Number: AM5708 Hi:
I have a AM5708 custom board with SDK5.02. I have implemented PTP over GMAC and am using timer13 for PPS output.
I have just moved to SDK6.02 and have realized that timer13 is not properly initialized by Linux, in fact I have…
Part Number: AWR1843AOP
Tool/software:
Hi team,
This is Lina covering Radar in Korea.
My customer designs an Automotive Side door system using AWR1843AOP for targeting HKMC.
They would like to use another XTAL(made by KDS:7AF04000A0W) without…