Part Number: SN65LVDM176 Hello,
I am using a COTS FPGA solution system containing the TI SN65LVDM176 to test an m-LVDS transceiver in a simple non-multipoint application. On another forum, it seems that this LVDM transceiver may be compatible with m…
Other Parts Discussed in Thread: SN65LVDM050 Related Case No.: CS0253265
Dear TI support, On our board, we are SN65LVDM050QDQ1 part to provide communication protocol (clock + data) between two FPGA devices. The clock operates at 100MHz (e.g. 200Mbps…
Hi Philippe,
Please help see SN65LVDM050-Q1 with an additional channel and more throughput or SN65LVDM1676 with up to 16 channels and less throughput, thanks.
Best Regards,
Michael.
Hi Craig,
The interfaces are different, M-LVDS does not require termination at every receiver like you have now and use 50 ohm differential opposed to 100 ohm for regular LVDS. M-LVDS should be able to support you 21 boards. I suspect that phase alignment…
Thanks Mike.
The reason we wanted to see the schematic is we got confused about the
· Internal Input 50-kΩ Pull-Down Resistor ?? Is the internal pull down for all PECL diff input. If so, why we need external pull up and pull down?
Also, we are…