Part Number: TAS5508C Other Parts Discussed in Thread: TAS5508 , TAS5558 , TAS5548 , TAS5352A We use the TAS5508C and we measured a delay between channels. We used differnt Chips which all showed the same result.
We could measure a delay of 2,7us between…
Part Number: TAS5508C Hi Team,
My customer plan to use TAS5508C, and they need to set loudness, Do you have good application note or reference for the tas5508c loudness?
Best regards,
Part Number: TAS5508C Hi Team,
My customer wants to use the DRC of TAS5508C limit output power ,How to configure the DRC parameters?
Thanks and regards
Part Number: TAS5634 Other Parts Discussed in Thread: TPA3255 , TAS5558 , TAS5548 , TAS5508C , TAS6584-Q1 The datasheet for the TAS5634 indicates that the minimum PWM frame rate for the device is 352Khz. It does not however describe anywhere what will happen…
Part Number: TAS5508C Other Parts Discussed in Thread: PUREPATHCONSOLE , TAS5548 Hello experts,
My customer plan to use TAS5508C, and they need to set EQ which they want to implement.
TAS5508EVM's GUI has some sample, but it can't set EQ which they want…
Part Number: TAS5508C
Hello
My customer is using TAS5508C and in the market.
It may be special case, but customer has pop issue from the market
in case very low level sound with low volume .
So far, customer had been set 0x14 as 14h [ D4=1].
When customer…
Part Number: TAS5508C Other Parts Discussed in Thread: PCM1808 , TAS5508 Hi,
We planned to use audio PWM Processor TAS5508C in our new project, We need to implement 8 channel ADC wIth TAS5508C.
The current concept is four PCM1808 used as the input channels…
Part Number: TAS5508C
Hello
My customer is using TAS5508C for their product.
When input source was changed, clock error will be occur, and small pop is heard from speaker even no music.
I attach the capture.
They set 0x04 PWM Automute = disabled.
They…
Part Number: TAS5508C Other Parts Discussed in Thread: TAS5558 Dear Support
The customer used TAS5508C and they want an output channel can be changed to Analog or I2S interface
Do you have any solution can do it?
Other Parts Discussed in Thread: TAS5508C Hi Engineers,
I would like to stop PWM output channels which is unused individually for TAS5508C.
How do i get it?
Regards,