Dear Derek -
One solution would be to use an I2C mux, which could be designed with this simple 2 channel device, which would allow you to put up to four TMP117s on one channel, and the remaining on the second channel: https://www.ti.com/product/TCA9543A…
Other Parts Discussed in Thread: TCA9543A , TMUX1072 Hi,
I am currently considering using the TCA9543A, but this chip requires I2C commands to select between Channel 0 and Channel 1. I and looking for an equivalent mux/switch that can select between…
Hi Evan,
Could you see if the TCA9543A can be used in your application? I would note that this device is capable of operation up to 400KHz however.
Regards,
Jack
Part Number: TCA9548A Other Parts Discussed in Thread: TCA9534A , , TCA9534 , TCA9543A Hi,
I'd like to confirm this, can TCA9534A support 1.8V as input, 3.3V as output application?
Thanks.
BR
Mason
Part Number: J721EXSOMXEVM Other Parts Discussed in Thread: DRA829 , TDA4VM , TCA9543A , CDCI6214 , TCA6416A , TCA6424 , TCA6416
Hi
Is there any developer guide exist for PCIe Root complex initialization sequence on TDA4VMXEVM ( J721E DRA829/TDA4VM…
Part Number: PCA9545A Other Parts Discussed in Thread: TCA9543A , SN74LVC2G66 Hi team,
This is Andy, FAE of Inspur Group.
Inspur is using our PCA9545A at Server, and I have some question on how use PCA9545A, please help me check.
1. PCA9545A have…
Part Number: P82B715 Other Parts Discussed in Thread: TCA9543A Dear team,
My customer is looking for a solution to communicate with the sensor board that is 2 meters away from the main board.
Firstly, I recommended to use P82B715 but the customer…
Hi Kay,
I think you should only need one TCA9543A near the master (or at a junction point between the two sensor boards), though two would work as well.
I have no expertise with the TCA9543A, but looking at the datasheet I would suspect that if you…
Part Number: TCA9546A Other Parts Discussed in Thread: TCA9543A , PCA9306 Hi there,
My customer is now using TCA9546A in one of their projects. However, they're complaining that the size is too big.
Since they only need two channels, I found TCA9543A…
Hey Minglai,
PCA9543A should be high impedance (or open as you call it) on SDA/SCL if no channels are enabled (selected) when it is turned on. Please ensure though you meet the Vcc ramp requirement specified in section 11 of the datasheet though because…