Hii,
we are working on an EV charger we are using MPS430 for the Digital feedback loop,
we required the design files and firmware of TIDA-00704 or TIDA-00703.
the data regarding TIDA-00704 for reference to our design.
Part Number: TIDA-00704 Hi Experts, Tried to design a charger using TIDA-00704 (w/o MCU) for 28.8v, 20Ah battery, I have two questions 1. How can I control the output voltage and current of TIDA-00704? via FB pin on U8 or via Vref and Iref of U5 and how to…
Part Number: UCC24610 Other Parts Discussed in Thread: UCC29950 , LM258 Team,
TIDA-00704 was designed to support output voltages of 20 to 32V. We have a customer who needs to know how this should be modified to support 12V out.
This design uses UCC24610…
Part Number: TIDA-00704 Hi all, I want to design a smps which need 30V 9A , and I just check TIDA-00704 performance is quiet fulfill my target, so I want to understand more about this design:
1. I checked that tiduc71a.pdf, the efficiency chart in page20…
Part Number: TIDA-00704 I have successfully downloaded the CAD files for ALTIUM. The schematics and the PCB are good but there isn't an integrated library of the components used in the board and so, when i will redesign my custom board I can't speed-up…
Part Number: TIDA-00704 Hello,
I have a customer using this design and the altium files aren't convertible to OrCAD. Do we have OrCAD files for this layout or can we generate the files in Altium to be compatible with conversion to OrCAD?
Best, Nad…
Part Number: TIDA-00704 Dear Sirs,
I'm trying to reproduce your TIDA-00704. I've all that I need except some components (tipically capacitors, but not only) which are in allocation.
I am designing my custom battery charger that is very similar…
Part Number: TIDA-00704
I have a customer currently attempting to use the TIDA-00704 as a standalone charger (w/o MCU).
However, upon discharging battery and attempting to use the design for charging purposes, the design is not functioning as expected…