Hi Elsa,
Here is a reference design using this device: https://www.ti.com/tool/TIDA-00821
However, this is an older device, I recommend looking into bq79606a or bq79616 product folders as they come with higher robustness, features, etc.
Regards,
Taylo…
Hi Henar,
What exactly are you looking for? We have a typical application schematic in section 8.2 of the datasheet and also you can download an example here: https://www.ti.com/tool/TIDA-00821 .
Regards,
Taylor
Hello Brian,
The -0.5A and 1.0A limits are continuous current limits and if you use the UCC2808-2 to drive a pair of FETs the current is pulsed due to the capacitive nature of the gate to source connection. This means the average drive current is very…
Part Number: BQ76PL536A-Q1 As you have given a reference design for the part number BQ76PL536A-Q1 in TIDA-00821, it contains 3 BQ76PL536A-Q1 on the same PCB. Hence there is no need to isolate the SPI daisy chain between them. I want to design a circuit…
Part Number: TIDA-00827 Hi,
I checked the TIDA-00827 tool link, i couldn't find the schematic of the reference design. Some other file (IMPORTANT NOTICE FOR TI REFERENCE DESIGNS) is there in schematic link. Can you please resolve this issue?
http…
Goto TI website and seacrch for TIDA-00821. You will find the design guide.
if you are referring Z1 from datasheet then it's zener.
Again, check out tida-00821.
Hi User, The SPI can be isolated using parts such as the ISO7241C. An example is used on the SPI of the bq76PL536EVM-3. It is shown on the TIDA-00821 schematic page 5, the PDF file presently has a problem but it can be found in the TIDA-00821 CAD Files…