Part Number: TIDM-02002 Other Parts Discussed in Thread: PMP21495 Hi. I have a question about Transformers. You know the Transformers in "PMP21495" produced by Payton? It looks like 4 terminals in layout or circuit diagram, but it looks like 6 terminals…
Part Number: TIDM-02002
Hi,
How do you calculate Lr2 in the CLLLC resonant tank. I am not finding it either in the excel sheet or in the reference guide. Could you please guide me on the same.
Regards,
Part Number: TIDM-02002
Hello. I'd like to ask you a theoretical question. TIDM-02002 is DC/DC converter
On the primary side, to convert DC to AC(pulse) its duty must be 50%. i understand this.
On the secondary side, to rectify AC(pulse) to DC, i…
Part Number: TIDM-02002 Hi Team,
Would you kindly confirm which of the codes ( TIDM_02002 v2.00.03.00 or TIDM_02002 v1.01.00.00) have current loop control and voltage loop control?
Can you also guide me to the best approach to implementing the current loop…
Part Number: TIDM-02002 Hi team,
We have reference design TIDM-02002 which is CLLLC topology. My customer's system is residential ESS in solar system, the battery voltage is about 48V, the HVDC voltage is about 400V. My customer has a question about…
Part Number: TIDM-02002 Hello this is Bumsu.
in the use of TIDM-02002, i have some difficulties as follows, so i want to get your proper advices on that.
as far as i understand, user can control the duty by changing CLLLC_pwmDutyPrimRef_pu and CLLLC_pwmDutySecRef_pu…
Part Number: TIDM-02002 Assuming that I put the Rogowski coil on the secondary side in reverse, should I invert the output from the comparator from this:
void CLLLC_HAL_setupSynchronousRectificationAction(uint16_t powerFlow)
{
if(powerFlow == CLLLC_POWER_FLOW_PRIM_SEC…
Part Number: TIDM-02002 Other Parts Discussed in Thread: PMP21495 , PMP21999 Hi all I noticed there is a difference in transformer values and inductor arrangement used in the design guide vs the values in the schematic. In the design guide there is separate…
Part Number: TIDM-02002 Other Parts Discussed in Thread: POWERSUITE
Hello,
I am currently developing the controller for (CRD-22DD12N) 22kW Bi-directional High Efficiency DC/DC Converter. Does the same control scheme used in TI TIDM-02002 board viable…
Part Number: TIDM-02002 Hello, everyone.
In the use of TIDM-02002, i setup the trip voltage > 30V , trip current >20 at the power stage.
But as i increase my power supply and when it reach Vprim=14[V] Iprim=1[A], CCS get doesn't work as like when it…