Part Number: TLV62565 Hi team,
My customer is used input 5.2V, output 3.3V. Some working conditions happen burned on top of the device scenario when powering up. So customer simulated direct short circuit of the output, but no burning out the chip. They want…
Part Number: TLV62565 Hello,
There're some question about the EN pin behavior.
1. We’re confused about the VIH/VIL definition of the TLV62569P and TLV62565. In the d/s, it would be something wrong on max. and min value. Please find the attached.…
Part Number: TLV62565 Hi TI Team,
Thank you for your support.
One of our customer complained,
He saw different date code parts in the one reel supposed to has only 1A and 25 (date code).
↓
He said there is "1C" and "1A". …
Part Number: TLV62565 Other Parts Discussed in Thread: TPS62825 Hi team, My customer would like to add a thermal pad on the TLV62565DBVR to heat dissipation. So, they need to know the weight bearing of the IC. I couldn't find it at Quality, reliability…
Part Number: TLV62565 Other Parts Discussed in Thread: TLV62569 Hi team,
I have a question about the FB resistor.
My customer would like to avoid the power save mode, so they're considering to flow dummy load by reducing the FB resistance. How low can…
Part Number: TLV62565 Hello team,
I got the questions from the customer about Webench sim. Could you support those below?
*Customer setting is that Vin:3.3V, Vout:1.5V, Rfbt: 180k, Rfbb: 120k
1: For load transient sim, Vout is a little bit high(1.518V…