Part Number: TMDSCNCD280025C Hello! I wanted to implement basic uart. This is the program that I've written. I'm stuck on how to display the values of different variables by using %d, %s etc. In the program below, I've printed a basic string.…
Part Number: TMDSCNCD280025C Other Parts Discussed in Thread: C2000WARE Hello, I am doing a project where I am planning to use the TMDSCNCD280025C for a battery management system.
I was wondering where I can find the schematics for this evaluation module…
Part Number: TMDSCNCD280025C I am currently trying to connect to the control card mentioned above via a USB connection without a docking station. When attempting to use CCS to connect to my board I am given the error "2131 - Unable to access device register…
Part Number: TMDSCNCD280025C The TMDSCNCD280025C datasheet mentions that there are 8 High Resolution PWM channels out of the 14 PWM channels. However I can't find any information on which of those 14 PWM channels are the High resolution channels. If anyone…
Part Number: TMDSCNCD280025C Hi,
<Phenomenon> In the past, the debugger and target were successfully connected, but a connection error occurred immediately after loading the program, and the target could not be connected after that. I did the following…
Manu36 said: Is it plan to have an updated document with all the parameters?
No plan to update the InstaSPIN user's guide. Most of the parameters in Universal lab are for the additional engineering features, not related to the FAST estimator. We only plan…
Part Number: TMDSCNCD280025C Other Parts Discussed in Thread: TMDSHSECDOCK , CODECOMPOSER I have the control card plugged into a TMDSHSECDOCK docking station and it's been working fine with the on-board XDS100v2 USB interface. However I want to verify that…
Part Number: TMS320F280025C Other Parts Discussed in Thread: TMDSCNCD280025C
Hi Team,
TMS320F28002x supports InstaSPIN-FOC.
My customer wants to use InstaSPIN gui with TMDSCNCD280025C and their motor to confirm motor control parameters
How to…
Part Number: TMDSCNCD280025C Other Parts Discussed in Thread: C2000WARE
I have been working on SPI Boot mode for C20025C. I have an external Flash connected to my DSP control card(TMDSCNCD280025C) over SPI.
So, the procedure I am following is this.
…
Part Number: TMDSCNCD280025C Other Parts Discussed in Thread: TMDSADAP180TO100 , I am currently running our 1 HP motor on TI’s HV kit with the use of Universal Motor Control Project. We are facing one problem in Level 3 build.
Our observations are…