Part Number: TMDXHVMTRKIT5X I bought a TMDXHVMTRKIT5X and HVPMSMMTR, follow doc(QSG-TMDSHVMTRKIT5X-GUIv1) step by step to make motor running,but there are some probems:
1/Motor's earth pin is floating, when i touch the motor ,I get an electric shock,but…
Part Number: TMDXHVMTRKIT5X Tool/software: Code Composer Studio Hi,
I'm just starting to use InstaSPIN_foc. How can I record the graphs obtained for the device test?
I would be glad if you can help
Part Number: TMDXHVMTRKIT5X Tool/software: Code Composer Studio Hello,
I am having problem identifying the motor when studying at lab 1b. Motor parameters are incorrect when I perform the motor identification steps. And the motor is not working. Where am…
Hi Anne, This PCB baseboard is shared between several kits (the TMDSHVMTRPFCKIT kit, the TMDSHVMTRINSPIN kit, and the TMDXHVMTRKIT5X). In the 5X kit, pin 57 is used as a DAC and it is used to generate an offset voltage for the F2805x's PGAs (programmable…
Hi Nimash,
The DRV8312 contains internal FETs. It is not designed to run at such high voltages.
The schematics can be found in controlSUITE. Once downloaded and opened, search for DRV8312 and locate the Hardware Development Package.
Schematics of a…
Hi Andrey, How to sense the current without glitches: The way around this is to trigger the ADC conversion based on the PWM waveform. If we can trigger the ADC SOC to occur once each period, while the bottom-side FET is on, the ADC data we get will always…
Thanks, since that's the schematic for the PFC TMDSHVMTRPFCKIT Kit (Piccolo F28035 & Delfino F28335).. is the output driver stage the same across all the high voltage kits, with just different control cards (TMDSHVMTRINSPIN (F28027F) or TMDXHVMTRKIT5X…
Other Parts Discussed in Thread: TMDSHVMTRINSPIN , CONTROLSUITE , TMS320F28035 , TMS320F28335 , TMS320F28069M , TMS320F28027F , MOTORWARE Hello all, I am trying to get information on the following:
#1 TMDSHVMTRINSPIN #2 TMDSHVMTRPFCKIT #3 TMDXHVMTRKIT5X
Q1. If…
Hello, Please note that there are two versions of this board which utilize the same PCB. It will be helpful to know which your are using. (1) is built around the 'F2805x series of C2000 MCUs - in order to utilize the on-chip PGAs (TMDXHVMTRKIT5X) \controlSUITE…