Part Number: TMUX1104 Team,
Customer is settingTMUX1104DGSR into AVL in their system, thus needs to understand below information for the device which some are not stated in the datashhet. Could you help to take a look and advise? Thanks.
Packing Type(Bag…
Part Number: TMUX1104 Other Parts Discussed in Thread: SN74HCS238 , TPIC6C595 Dear Team,
May I know the output current capacity of TMUX1104.
Regards
HARI
Part Number: TMUX1104 Dear e2e team,
I'd like to know which is the suggested soldering profile for TMUX1104DQAR and if it is different than the STD jedec J-STD-020.
Thanks,
Giorgia
Part Number: TMUX1104 Other Parts Discussed in Thread: TMUX1108 Hello TI Member:
I would like to use TMUX1104 as a programmable circuit to measure the current consumption, and the order of quiescent current is about 10nA.
Since the leakage current of…
Part Number: TMUX1104 Other Parts Discussed in Thread: TMUX1108 , TMUX1109 Dear Team,
We are using TMUX1104DGSR in one of our projects.
Currently, it is not available with any of our vendors.
Could you please suggest an alternate P/N for the same?
Reg…
Part Number: TMUX1104 Hi,
Could you please let me know if TMUX1104DGSR is a Pin to Pin replacement for MAX4734EUB. If not, what is the best replacement device you can recommend.
Regards, Sandesh
Part Number: TMUX1104 Dear Team,
We are looking for an on/off switch for ethernet signals (1Gbps) .
Please refer to the block diagram below.
MUX is used to switch WAN signals to WAN1 or WAN2, but it seems that there is signal interference between WAN1…
Part Number: TMUX1104
Hello TI Member:
We would like to use TMUX1104 to make a multiplexing gate circuit with operating frequency up to 50MHz.
However, there is leakage current at 5MHz, which affects the use. We do not know the reason.
Have you ever…