Hello Mike,
Thanks for the extra info and I think I understand your question. I wanted to clarify and state that this device is rated to handle io signals 0 to 3.6V
So to answer part of your question ,TI multiplexers can handle your scenario which is…
Part Number: TMUX136 Tool/software: Hi,
Can i use this mux for CVBS and 3G- SDI signal switching
CVBS Frequency is around min 3.5MHz NTSC and PAL 4.4MHz ,This is a analog signal . the 3G-SDI is a digital signal which has the frequency of 1.25GHz. It should…
Part Number: TMUX136 Tool/software: The datasheet specifies that the switching time from SEL to output is at most 600 ns. Is this just a latency or is there additional time for the outputs to settle? In other words, if COM is connected to A and SEL toggles…
Part Number: TMUX136 Hi Team,
Can you please share layout guidliness for I3C.How much stub length is okay for I3C which will be work on 12.5Mhz.
Many Thanks
Rajat
Part Number: TMUX136 I'm trying to use TMUX136 as a multiplexer for UART channels, I have a requirement such that the device should have a default state when VDD = 0, I don't want the channel to be in high impedance state. Is it possible with the multiplexer…
Part Number: TMUX136 Other Parts Discussed in Thread: TCA9548A Hi Team
do TI have any solution to replace R3GMxxB12?
https://www.renesas.com/us/en/document/sds/rg3mxxb12a1-short-form-datasheet
It's I3C switch +HUB
BRs
Brian
Hi Drew,
Thank you very much for your answer, I believe I now have all the information I need to continue my design :).
Also, thank you everyone else for your help.
Kind regards
Wes
Part Number: TMUX136 Hi,
I am looking for some clarification on the maximum allowable current into the TMUX136.
The datasheet states it is +/- 20mA Continuous. What is the maximum pulsed current and duration of this ? or is it simply that the pulse current…
Part Number: TMUX136 Hello,
On TMUX136, can I connect the OE pin directly to ground? Or should I place a resistor between the pin and ground?
Thank you!
Best regards,
Zach Kimble