Part Number: TMUX1511 Other Parts Discussed in Thread: SN74CBTLV3126 Tool/software: Hi team.
Do we have p2p replacement for 74CBTLV3126BQ,115? Thanks!
Nison
Hello Morteza,
Thanks for the response and let me try to explain what I know based of my understanding.
1.From what I have read you can use equalizers in single ended configuration by terminating the unused input and output.
2.I am not sure about this…
Part Number: TMUX1511 Other Parts Discussed in Thread: LMH6574 Hello TI, i have a small doubt that is TMUX1511 it will support to two HD-SDI video input And two NTSC/PAL video input and one output. can u give reply fast.
Hello Morteza,
I am not a high speed PCB designer, but here are a few suggestions
1.First , what you could do is remove the mux and put a discrete RC low pass filter on the board to represent the mux signal path.
2.Next, You could test the board by removing…
Part Number: TMUX1511 hi,
Fout2 inputs a frequency square wave from 10KHZ to 100KHZ, and SEL1 and SEL2 are both high or low levels. SEL3 and SEL4, due to the connection of inverters, have opposite levels to SEL1 and SEL2. When SEL1 and SEL2 are high,…
Part Number: TMUX1511 hellow
I would like to know the change of 10℃ interval of TMUX1511 (DVDD = 3.3V -40~125℃). Datasheet from Ttransition VS Temperature is present in Datasheet, but the Temperature impact of Ton/Toff could not be verified. Best Regards…
Part Number: TMUX1511 hi,
When Fout2 connects signals from 10KHZ to 100KHZ, the measured TP10 and TP11 are a set of reverse frequency signals. A 1pf capacitor is welded at the position of C31, and the voltage TP13 0.0024V TP15 0.0015V TP16 0.0015V TP17…
Part Number: TMUX1511 Other Parts Discussed in Thread: TMUX2889 , TMUX4827 , TS5A22362 , LM7705 Hi TIer
1. Could TMUX1511 transmit negative voltage? (When use single ended power supply)
2. When customer use 5V power supply , The channel generates a 7V pulse…