Part Number: TPS2595 Hello I would like to use a TPS259573DSG to set a custom 5.5V overvoltage lockout threshold (OVLO) with a 5 Volt input (normal, during fault it will be 7-8V which would damage the load thus why I am using an eFuse) How would I set a…
Part Number: TPS2595 Hi team,
can you please provide the correct pSpice model for TPS259573 device. I checked in the website it is shown differently behaviour and it pspice is written for UVLO instead on OVLO.
where as datasheet shows as below,
…
Part Number: TPS2595 Hi TI team,
we received below material with MSL 2, but our system + your website shows MSL 1. could you check why ship with different MSL.
BatchNo
PartNo
VenderNo
Vendername
MFG
MPN
Qty
OrderNo
issuecategory
…
Part Number: TPS2595 Other Parts Discussed in Thread: TPS2596 , TPS1641 , TPS25961 Dear all
I'm designing a board that has to work at 3V, 150mA max and any current over 250mA is considered a shortcircuit
On the other hand, I have to monitor the current…
Part Number: TPS2595 Other Parts Discussed in Thread: TPS2597 Hi team,
My customer wants to output continuous 4A with TPS259531DSGR, considering variation. So my customer wants to use Rilm=470Ohm. But it violates the recommended operating conditions. Should…
Part Number: TPS2595 Hello Team,
may I kindly ask you for an explanation why the same package has different MSLs, please?
Thank you and Best Regards, Hans
Part Number: TPS2595 Hi team,
Is customer able to add diodes to prevent below?
1. Reverse current blocking: Is it ok to add diode to prevent it?
2. Reverse polarity: Is it ok to add Schottky on input? If it works, Vin would be < -0.3V.
BEst regards…
Part Number: TPS2595 Hi team,
There is a equation to set ILim. Is the 2000 and 0.04 typical value? How can I estimate the real Ilimit accuracy?
If we can not comment on the each value&s accuracy, please let me know the Ilimit fluctuation value such …
Part Number: TPS2595 Hi,
I have a customer who used TPS2595 before, but now wants the current to be limited to about 1.5A and the voltage to be between 0.8-8V. Is there any suitable overvoltage protection chip recommended?
Many thanks~
Part Number: TPS2595 Other Parts Discussed in Thread: TPS25947 we need an overvoltage controller for a 3.3V supply.
Our first approach is with TPS259573.
The rising threshold level on EN/UVLO-Pin is acc. to datasheet: 1.2V ±70mV.
With these tolerances…