Part Number: TPS3703-Q1 Tool/software: we purchased the part#TPS3703B3080DSERQ1 from Mouser,but the pins of TPS3703B3080DSERQ1 are yellow,
the customer suspects that the parts may oxidize. the customer want to return the parts to Mouser.pls help to check…
Part Number: TPS3703-Q1 Are 3.3v VDD and logic driving MR# input for TPS3703C7500DSERQ.compatible when monitoring a 5v power rail or VDD needs to be =< Vsense?
Part Number: TPS3703-Q1 Other Parts Discussed in Thread: TPS3703 I have three TPS3703A4080DSER to share only one VCT pin from FPGA as below. The three Reset# pins are seperated.
I found only when all three Reset# changed to low level, VCT can unlatch the…
Part Number: TPS3703-Q1 Hello,
Support requested for understanding the issue.
We have used the chip TPS3703B4250DSERQ1 in our design. While testing the board, we have encountered the issue that the reset is not releasing. 5V power line is stable.
Design…
Part Number: TPS3703-Q1 hi,
There is a equation like this in 9.1.2.2 Programmable Reset Delay-Timing
td=3.066 x Cct +0.5ms if Cct=0.1nF, the td=0.8066ms
how can this match to this table? the typ td is already more than 5ms, but calculation gives less…
Part Number: TPS3703-Q1 Hi Team,
I have questions about the TPS3703-Q1. If the SENSE voltage is from 5.5V to 6V, does it work normally? I know we cannot garantee the spec due to over the recommended operating range. but we want to just know the behavior…
Part Number: TPS3703-Q1 Other Parts Discussed in Thread: TPS3703 ,
Hi team,
Could you help recommended the high accuacy voltage detection reset IC?
The TPS3703 would be a perfect solution for the application, but the voltage need to be monitor is 1.…
Part Number: TPS3703-Q1 Hello, I'm struggeling a bit with the parameters sense glitch immunity (tGI) and detect propagation delay (tPD). How are both related to each other? If we consider e.g. an undervoltage / overvoltage condition for 100us and measure…