Part Number: TPS3890-Q1 Other Parts Discussed in Thread: TPS3899 Hi,
I am looking for a supervisor or pushbutton controller that has a programmable output delay and monitoring input setup time.
Specifically, I am looking for a device that can monitor the…
Part Number: TPS3890-Q1 Hi team,
My customer want to know tPD(r) min/MAX value. In the datasheet there are only nominal value.
They want to calculate by using min/MAX value. Not NOM.
Regards,
Youhei MIYAOKA
Part Number: TPS3890-Q1 Hi Expert,
May you kindly help share the CTE(Coefficient of thermal expansion) value of TPS389030QDSERQ1 and TPS389025QDSERQ1?
Thanks!
Ethan Wen
Part Number: TPS3890-Q1 Other Parts Discussed in Thread: TPS3890 , I have a question is about component TPS389050GQDSERQ1. We have the following datasheet for it: tps3890-q1-Feb_2018.pdf (SBVS303B –MARCH 2017–REVISED FEBRUARY 2018).
Additionally…
Part Number: TPS3890-Q1 Hi
May i know how to get below data for TPS389030QDSERQ1
Thermal expansion coefficient,
Heat capacity,
Heat conduction coefficient,
Heart flux from IC chip 6 faces
Part Number: TPS3890-Q1 Hello!
Is it possible to supply higher voltage on MR/ pin than VDD?
I want to supply 1.8V on VDD pin and 3.3V pull-pu on the MR/pin.
Part Number: TPS3890-Q1 Other Parts Discussed in Thread: TPS3808-Q1 Team,
Can you use one of the TPS3890-Q1 with an external divider on the sense pin to achieve a trip threshold of 0.9V?
Part Number: TPS3890-Q1 Hello,
could you please clarify, if it is allowed to apply 3v3 to the MR_, having VDD=1v8?
Or what effects have to be considered while applying a higher voltage to MR_ compared to VDD?
Best Regards, Martin
Part Number: TPS3890-Q1 Other Parts Discussed in Thread: TPS3890 Hello,
I'm looking for a reset IC that can realize a delay time of 80 ms +/- 10 ms. From the equation of TPS3890-Q1, we couldn't achieve 80ms +/- 10ms delay time. Please see the attached…
Part Number: TLV840-Q1 Other Parts Discussed in Thread: TPS3890-Q1 Hi expert,
What's the VIT- and VIT+ for TLV840MADL30DBVRQ1? In TPS3890-Q1, we have a table as below, but I didn't find such kind of table in TLV840-Q1. Thanks.
Arie