Other Parts Discussed in Thread: TPS40400 , TPS40077 Hi Team, My customer wants PSpice model for the following controllers. Do you have PSpice model for these devices? - TPS40400 - TPS40077 Best Regards, Yaita / Japan disty
Michele,
AVS use is mandatory. This is stated multiple times in the Data Manual excerpts above. TI cannot guarantee reliability targets will be met without use of AVS. TI provides example AVS drivers in both EZSDK and the RDK code branches. The RDK…
The UDWorks board is controlled through I2C.
The recommended solution for power management is the TPS40400.
Then the EVM was generated the TPS40400 was not in production.
Some form of AVS is required and the only TI supported method is with the…
Part Number: TMS320DM8168 Other Parts Discussed in Thread: TPS40400 , PMP Hi,
We have a product developed around TI8168 based on DVRRDK_03.50.00.05. My question is regarding smartreflex feature. We use an I2C controlled voltage regulator TPS40400 in…
I am waiting on the board. In the meanwhile I checked the TPS40400 and it responds within 2-5us. Typically it would take 2-3 clock cycles for frequency to lock in.
So for example a 500khz sync pulse (2us periode) would change the switching frequency…
The kernel log doesn't show the tps40400 regulator initialized. Do you have tps40400 on your board as mentioned in design guidelines and are you pluging in the regulator correctly in your kernel configuration ?
Hello Di,
I would need some more schematic information on what you are correcting with the sensed voltage, but when the load changes, the voltage of your power IC or buck converter will ring proportional to the power stage bandwidth. So if the instrumentation…
Other Parts Discussed in Thread: TPS40400 , CSD87350Q5D , CSD87384M Dear All,
My customer is now using PowerBlock CSD87350Q5D. Cntroller is TPS40400. For next Model, they want to evaluate PowerBlock II CSD87384M and got sanples.
Q1) Is surface fin…
Other Parts Discussed in Thread: TPS53915 , TPS549B22 , TPS546A24A , TPS40400 , TPS40422 , TPS40425 Hi Team,
Could you pls suggest suitable parts for the requirements, thanks
(PWMs have PMBUS -- Vin 12V , Vout 1.0v 1.8v 3.3v MAX 3A)
Other Parts Discussed in Thread: TPS40400 Hi, We are developing DM8168 based IP camera. It has TPS40400 PMIC chip. We ported EZSDK to our platform, but it dont have TPS40400 PMIC driver, we took same from RDK 3.5. When booted camera, we can see s_hvt…