Part Number: TPS54340-Q1 Hi Team,
There is a good new that we could DIN TI product! But cause TPS54340QDDARQ1 is out of stock !
Could you help find out alternative solutions for the parts below? (can be supplied normally at present would be better ) TH…
Part Number: TPS54340-Q1 Hi,
Whether the current limit of TPS54340QDDARQ1 varies with the temperature? If so, Please provide the current limit for the following temperatures
1)Tamb: 105C
2)Tamb: -40C
Thanks
Viswa
Part Number: TPS54340-Q1 Hi Team,
One of my customer using this device have below query during over current operation. Please help with output voltage to output current graph (Or Input v Output current)
If the load draws 3.5A< Iout < 6.8A, will the Regulator…
Part Number: TPS54340-Q1 Other Parts Discussed in Thread: TPS54340B-Q1 , Hello,
What exactly is the difference between NRND TPS54340-Q1 and its replacement TPS54340B-Q1?
Part Number: TPS54340B-Q1 Other Parts Discussed in Thread: TPS54360-Q1 , TPS54340-Q1 , , TPS54360B-Q1 Dears:
Our customer uses TPS54340-Q1 and TPS54360-Q1, and these PNs are NRND.
I promote TPS54340B-Q1 and TPS54360B-Q1, there is an issue about the design…
Part Number: TPS54340-Q1 Other Parts Discussed in Thread: TPS54340 Dear Sir/Madam
How much is the maximum current that this IC can handle. My requirement is to generate an output of 36V with a maximum load current of 3A from a 22 to 30V DC input. whether…
Part Number: TPS54340B-Q1 Other Parts Discussed in Thread: TPS54340 , TPS54340-Q1 , Hello,
what's the difference between TPS54340 B -Q1 and TPS54340-Q1?
Best Regards
Martin Grimmer
Part Number: TPS54340-Q1 Other Parts Discussed in Thread: TPS54340B-Q1 , Hi, team.
What is the difference between TPS54340-Q1 and TPS54340B-Q1?
Best Regards,
Kobayashi
Part Number: TPS54340-Q1 Hi,
Im trying to use the below equation for Vstart and Vstop voltage calculation.
But its not matched with the actual value arrived.As per the above equation,If Vstart=5.75V and Vstop =4.5V.
Ihys=3.4uA. then RUVLO1 value should…