Part Number: TPS560430-Q1 Tool/software: Hi Team,
My customer Meta System is testing the unencrypted model of TPS560430-Q1, but they get below error. Can you advise how to solve?
Also, they said they need long time to stabilize the output, do you have…
Part Number: TPS560430 Other Parts Discussed in Thread: LM61495-Q1 , LM61440-Q1 , TPS552872-Q1 , TPS628503-Q1 Tool/software: Can you share the SIMPLIS model of the parts list below?
<parts list>
No.
DC/DC
1
LM25148QRGERQ1
2
LM61495-Q1
3
L…
Part Number: TPS560430 Tool/software: Hi,
I am trying to run simulation of TPS560430Y_TRANS. I am getting this error message
Errors found during the run. Simulation aborted
*** ERROR *** Error in parameter expression 'rvtoi_hs/pk2vl' (Line ref: TPS560430Y_TRANS…
Part Number: TPS560430-Q1 Tool/software: Hi team,
I tested the bode plot on customer's board. It was strange.
I think it is because customer did not solder a wire on 50 ohm+. I had to link the test device to Vout pin.
Do you have a bode plot result…
Part Number: TPS560430-Q1 Tool/software: 1538.5V,600mA Reg.pdf I have attached a schematic design with the input voltage of 12V and output voltage as 1.5V with the current rating of 600mA. Can anyone please confirm the design is correct or if any changes…
Part Number: TPS560430 Tool/software: Hi Ti Team,
We are using 2 pieces of TPS560430 to generate respectively +5V and +3v3.
The two TPS560430 are located in two different board which are linked togheter and they both receive the same +12V as input
The two…
Part Number: TPS560430 Other Parts Discussed in Thread: SN65HVD235 , TLV9154 Hello,
we intend to use the TPS560430X to convert 24V Vin to 5V. From these 5V we use an LDO TPS70933 for 3.3V.
We need the 5V for some OpAmps and the 3.3V only to power a small…
Part Number: TPS560430 Other Parts Discussed in Thread: LMR51610 Hi Colleagues,
Could you offer similar device to TPS560430 with input voltage greater than 36V?
P2P would be ideal.
If there is no P2P, can you recommend best alternative device?
Thank you…
Part Number: TPS560430-Q1 Hi,
can you let me know the failure mode to be consider for TPS560430-Q1.
Also what is failure mode distribution for the above IC.
Thanks and Regards,
Mangesh