Thanks for your feedback. TPS60400 has relatively high device Quiescent Current, Typical 65 µA. The system I am working on should operate at less than 1mA, this include op-amp and ULP MCU ruing at 2MHz. That is why I am trying to use TPS26740 as voltage…
Other Parts Discussed in Thread: TPS60400-Q1 Hello,
Please suggest cost optimized automotive grade solution to create negative reference voltage of -1.35 V and -0.85 V from 3.3 V.
Thank you!
Hi Tomas,
Please give me the answer to another question sent to 6/28.
And there is another question:
-. How can use the +24V input voltage ==> +5V output voltage(max. 0.3W) solution.
Cannot be used Buck IC because the PCB size issue.
…
Alex,
Also, you used the inverter TPS60400 to create the negative voltage for the current mirror. Can an inverter be used to create the EA BIAS voltage or does it require more current capability?
Mike
It sounds like what are trying to do is create a +/-5V supply, for example? You usually keep the same system ground reference and create the voltages with switching power supplies. The TPS60400 is a simple inverter one.
You could use the TPS62080 to go from 5V to 4V or an LDO.
For the -1V rail, you could use the TPS62120 from 5V with this app note: www.ti.com/.../slva478b.pdf
Some customers use the TPS60400 charge pump (from the 4V rail) and then an LDO to get…
Other Parts Discussed in Thread: TPS60403 , TPS60400 Hello Ti-Experts, I built a simple buffer circuit using the TPS60403 for biasing with the 3 recommended 1uF capacitors from the datasheet. My load current idles at about 40 uA and swings around that…
I've not seen a single chip with a negative voltage but 2 discretes can do.
The TPS60400 family can easily make your -5V.
For the 3.3, the TPS82740B is the absolute smallest device. TPS62237 would be a discrete version but still small.
Other Parts Discussed in Thread: TPS60400 , OPA657 , TPS60401 Dear specialist
Our customer is considering TPS60400 to create from Vin5V to Vout -4.6~4.8V. They are also considering 2pcs OPA657 whose Iq per device is 26mA. If they used TPS60401 , could…
Hello Jared,
If you are searching for a part from 24V input voltage, I do not know of any in the portfolio I know, but we have several that are going from +5V to -5V, e.g. TPS63700 or TPS60400. And some that have 2 outputs, one positive and one negative…