Part Number: TPS62097-Q1 Dear TI colleagues,
TPS62097QWRGTRQ1 is a part of power supply chain of TimeOfFlight reference design with Melexis camera sensor. This means the customers of Melexis can see our validated design and became also TI customers by…
Part Number: TPS62097 Tool/software: WEBENCH® Design Tools Hello All,
I was trying to design a buck converter, which has Vin in the range of 4.5V to 6V, and Vout at 4V. The output current is at 2A. But when i try to design this using the WEBENCH, it is…
Part Number: TPS62097-Q1 Other Parts Discussed in Thread: TPS62097 Hi Sir,
Look into the datasheet of TPS62097-Q1, the EN enable pin VH and VL show as below,
Normally, on others converter, they will show Min. and Typ. for VH and Max. and Typ. for VL…
Part Number: TPS62097 Hi,
The TPS62097 web page says that this device is capable of Pre-Bias Start-Up. The data sheet says nothing. So which is it?
Does the TPS62097-Q1 support Pre-Bias Start-Up?
Best regards
Torbjörn
Part Number: LMR14206 Other Parts Discussed in Thread: TPS62097 LMR14206 failures issue
We have a design 24v/12v input to 5 v rail typically 20mA, max 100 mA using a LMR14206.
The 5 V rails feeds a TPS62097 Step Down Converter for the 3.3 V rail. Again…
Part Number: TPS62097-Q1 Other Parts Discussed in Thread: TPS62097 , Hi-
I've been looking everywhere and can't seem to find any guidance for layout footprints. Can you please point me in the right direction? Maybe a suggested footprint?
Thanks…
Part Number: TPS62097 Hi,
What ampere is current source of mode pin during MODE=Low?
I would like to know maximum resistance to pull-down mode pin under 0.4V.
Best Regards,
Kuramochi