Part Number: TPS62808 Other Parts Discussed in Thread: TPS7A21 , TPS7A03 , TPS7A02 , TPS7A05 Hi,
I would like to know the whether LDO (TPS7A2133BPYWDJ) or Buck (TPS62808YKAR) performs well with a Battery(Lithium Thionyl Chloride Battery) operated device…
Part Number: TPS62808 Hi,
I would like to know whether the given buck regulators can be used to step down voltage from 3.6V-3.3V with current of 500mA
1. TPS62808YKAR
2. TPS62802YKAR
3. TPS62840YBGR
Could you suggest some buck regulators or LDO that has…
Part Number: TPS62808 We are successfully loading and soldering parts for our prototypes, but I am looking for a TI recommended pcb pad, solder mask AND solder past dimensions. I didn't see anything in the technical lit, but I could have missed it. Thank…
Part Number: TPS62808 I need to create a -2.5V (Iout <= 0.1A) voltage using a battery voltage (3-4.3V). My design already uses a TPS62808 for another voltage. I am very space constrained and concerned about battery life so I am interested in using…
Hello Stefano, I believe our MCU can be supplied by the TPS62808 or from an LDO on the PCB. If we figure out we need the GPIO connection we will use a FET controller from the MCU connecting the EN to GND if we need to be able to turn the IC off in the future…
Part Number: TPS62808 Hello,
We're using the TPS62808YKAR in one of our designs. According to the table the device marking should be "V".
The regulators placed by our EMS however has the device marking "T", which does not exist in the table…
Part Number: TPS62808 hi,
is there any data or expectation while using 2.2uH as inductor?
I know we recommend 1uH max, just wondering if that has ever been tested.
thansk a lot
KR
Vincenzo
Part Number: TPS62808 Other Parts Discussed in Thread: TPS62743 , , TPS62840 Hi! Currently, I'm using TPS62743 to convert 5 V to 1.8 V to power a BME680 which has a peak current of 12 mA during the measurement. Because I can only draw 5 mA at maximum…
Part Number: TPS62808 Hi Team,
I would like to find the solution which meet below requirement . I find TPS62808 in ti.com. Do we have more appropriate solution? or next gen roadmap could send me directly?
Description
Vin
Vout
Iout
Efficiency…
Part Number: TPS62808
Dear Sirs,
I found the TPS62808 output voltage will higher than 1.8V if my output current is very low.(2mA)
As other E2E post, it seems the startup simulation is no problem.
However, the steady state simulation still have wrong…