Part Number: TPS63806EVM Hi,
I'm developing a regulators usign the mentioned IC and reading its datasheet I found this problem:
(in page 26)
But the pin function table says:
(in page 4)
which option is the correct one?
I got the datasheet from…
Hi Brad, When the TPS63806 is disabled via EN pin, its output is floating and there is only a small leakage current which should be well below 1 μA. The majority of the leakage current should go through the voltage feedback divider. Have you maybe modified…
Part Number: TPS63806 Hello,
I have some questions regarding the TPS63086 layoutL
1. One of the layout guidelines in the TPS63806 datasheet states to "use separate traces for the supply voltage of the power stage and supply voltage of the analog stage…
Hi Milos,
pls refer to the attachment, including the schematic and description, this test is on our TPS63806EVM, so the layout is same as this EVM. TPS63806-TEC Driver -.pptx