The slew rate from 0 to 1.4V is very fast --> 1.5V/12us = 0.125V/us. If this slew rate were constant, VDIG1 would reach 1.8V in 14us instead of 100us.
The slew rate from 0 to 1.4V should be ignored. This is how fast the VDIG1 would ramp if it were…
YF,
PWRON , SLEEP , and PWRHOLD input pins on the PMIC work together to determine when the TPS65910 turns on and when it goes to the ACTIVE, SLEEP, or OFF states. By definition, the TPS65910Ax OTP spins for Sitara AM335x do not wait for PWRON pin to start…
Taka-San,
Apologies for my delayed response, as I have yet to locate any relevant documentation over these specifics of the errata, and would have to re-create these conditions on an EVM. If your customer has a specific concern they can actually test…