Part Number: TPS7A05 Other Parts Discussed in Thread: TPS7A03 , TPS7A02 Hello Experts, My customer is considering to design to prevent reverse current condition. [reverse current condition] - Vin=0V - Vout=5V - workaround: see below block diagram. The ABS of…
Part Number: TPS7A05 Other Parts Discussed in Thread: TPS7A03 , Hi Team,
during test on TPS7A0528, we found below
Green= Vin, Yellow= Vout. Vin and EN pin are connected together.
1. there is a stage before Vout ramping up to Vset @ no load ( red circle…
Part Number: TPS7A05 Other Parts Discussed in Thread: TPS723 , LM337 Hi Team,
can you please check the request of my customer:
--------------------------------------------------------------------
We have a -3.3V supply and need to produce a -2.5V rail…
Part Number: TPS7A05 Other Parts Discussed in Thread: LP5907 , TPS7A88 Hi Sir,
My customer looking for LDO solution like TPS7A05 but fast star-up time around 50uS.
Do you have suggest which one is good for this?
Thanks, Ian.
Part Number: TPS7A05 Other Parts Discussed in Thread: TPS7A03 Datasheet statement: P is optional; P indicates an active output discharge feature.
Is it possible to have version without this feature ?
Interest in 2.7V Version SOT 23-5 preferred, SOT 23…
Part Number: TPS7A05 Other Parts Discussed in Thread: TPS7A24 , TPS7A20 , TPS7B69 , LP2985 , TPS784 , TPS784-Q1 Hi expert,
TPS7A05 was mass production on customer side. Now there is a new project need LDO. Here is the requirement, could you recommend a new…
Part Number: TPS7A05 Other Parts Discussed in Thread: TLV767 Hi Team,
I received an inquiry from a customer where they need a higher Vin version of our TPS7A05 with the same Active output discharge feature. Below are their requirements:
active output…
Part Number: TPS7A05 Hello
Could you tell me if the output voltage of the TPS7A0533PDBVT tracks the input voltage down below 3.3V? I'm looking to use it in a battery powered operation and it would be useful if it continued to output when the battery input…
Part Number: TPS7A05 Dear Sirs,
Customer test TPS7A0512 with SOT23-3 package and found while Vin low to 1.239V, the output will cut off.
Please help to clarify if using SOT23-5 package and force EN high in Vin=1.239V, the output will cut off, too?
Or…