Part Number: TPS92692-Q1 Tool/software:
Hello , I would like to know the following
1.) what is the function of Q2 PNP transistor in the application circuit shown in datasheet? how to select it?
2.) How is boost to battery and Buck boost topology different…
Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92692 Tool/software: Hi
Our customer has raised some questions about the TPS92692:
1, In the datasheet table2 gives the calculation formulas for G0, wp, wz, could you please tell me about Vo…
Part Number: TPS92692-Q1 Tool/software: Hi team,
I are turning off VIN with high side switch to minimize the current consumption. But I am concerning about Qm and Gate-pin status when IC is off. It may be undefined, so I think Gate-source resistor will…
Part Number: TPS92692-Q1 Tool/software: Hi Team,
The datasheet lists Typ values of PDRV delay, but are there any other MIN and MAX data available?
Also, if it is possible to obtain this information by calculation, please let us know how to do so. …
Part Number: TPS92692-Q1
Tool/software:
Hi team,
My customer uses 92692 in the constant current boost design, could you please give some comments for below question? Thanks.
The 5V LDO of Vref will be turned off when PWM is low? As shown in the picture…
Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92692 Tool/software: Hi Team,
My customer is evaluating TPS92692-Q1 in their project, could you please help give some comments for below questions?
When the customer is using the TPS92692 as…
Part Number: TPS92692-Q1 Tool/software: If "VIn" is off, What is state these pins?
・ GATE
=>
・ OV
=>
・CSP
=>
・CSN
=>
・PDRV
=>
exp)
Hi-Z? Low?( Internal pulldown?(Resistor value) )
Part Number: TPS92692-Q1 Tool/software: Hi,
I am working on sepic conerverter design for below spcification.
Vin 8V to 16V
Vout 21V
Iout 0.75A
Fsw: 400KHz
i am checking MOSFET drain waveform from 8V to 16V. Till 13V VDS signal is ok. when i cross 14V…
Part Number: TPS92692-Q1 am using PSPICE in Cadence Allegro 17.4. An error occurs in the simulation.
I using olb file of TPS92692-Q1 Boost and Buck Boost PSpice Transient Model (Rev. A) of TPS92692-Q1 data sheet, product information and support | TI.c…
Part Number: TPS92692-Q1 Other Parts Discussed in Thread: TPS92692 hello
when i use the TPS92692, i found that The start-up time of the chip varies with different PWM input duty cycles.
please refer to the follow picture.
the blue line is the input voltage…