Part Number: TPSM84212
Hello E2E,
Our customer is using the TPSM84212EVM-888 module and while using it the module burnt out. They're using a 24.8V on the input at 660mA and a preliminary load testing to ensure functionality using a lab-grade power supply…
Part Number: TPSM84212 Hi,
I would like to use TPSM84212 but its current capacity is a bit less than I would like to have. Does anyone know this module can be used in parallel to enhance output current and how?
Thank you.
Katsuhiro
Part Number: TPSM84212 Hi Team,
The minimum of input is 14.5V in TPSM84212EAB..If the input is 12V or less than 12V, will the output follow input.
customer could accept such situation A. For example, Vin =12V, Vout =11.9V.
But if Vin =12V, Vout =0V, customer…
Part Number: TPSM84212 Powered up with 24 VDC with no load and it failed. I have 3 that failed. It doesn't seem to like fast rising input power with high switch bounce. the power was connected using an ezehook which does make a clean connection if the…