Hi Team,
1) Cno(off) Off Capacitance is measured when the switch is not biased/powered?
2) How is ON capacitance for NC/NO measured? or how is these separated from COM capacitance? Wouldn't NC or NO capacitance include COM because the switch is always…
Part Number: TMUX1219 Other Parts Discussed in Thread: TS5A12301E , TS5A6542 , TPS2111A Hi Team, Our customer is asking for an alternate solution for TMUX1219. Their set-up requires a switching between S1 and S2 on two voltages (3.3V and 3V) as tests are…
Part Number: TS5A2066 Other Parts Discussed in Thread: TS5A12301E , TS5A9411 , SN74LVC2G53 Hello,
I was looking for the best replacement we have to the NXP part 74LVC1G53: assets.nexperia.com/.../74LVC1G53.pdf
On TI.com it said the TS5A9411 or the TS5A12301E…
Puchong,
You can search for signal switches using the ti.com switch search tool . Select the filters for configuration 2:1, channel = 1, Vdd > 5V and I/O continuous current > 200mA. The TS5A12301E has lowest Ron in BGA package and TS5A4624 is in…
Part Number: DRV2625EVM-CT Other Parts Discussed in Thread: TS5A12301E , DRV2625 The datasheet says that the J4 jumper allows me to connect to the I2C bus for "Debug/Monitor or Advanced Operations." I understand how I can easily use these pins to monitor…
Narek,
The power sequencing comment is in the datasheet for all passive CMOS FET switches. There are protection diodes on the signal path that can conduct to Vcc if the signal path sees a voltage before the supply. When these diodes conduct they can pass…
Part Number: TS5A3159 Other Parts Discussed in Thread: TS5A12301E , TS3A24157 Hello,
my customer looking for SPDT device that can provide up to 300mA. He used TS5A3159DBVR in the past, but unfortunately it can't support that current.
For the prototype…
Yazhu,
You are correct that this device doesn't have powered off protection like the TS5A12301E and Vcc must be within the recommended operating conditions before signals are placed on the I/O path.
A typical symptom of signals on the I/O path…
Shashank,
he TS5A3160 can be used to switch signals 0V to 2.5V . Why did you choose the TS5A3160? The TS5A12301E has lower on-state resistance than TS5A3160 and SN74LVC1G3157 is much lower cost.
The mosfet used in the TS5A3160 is both a P-channel and…