Part Number: TS5A3359 Hi, I would like to check if there are negative diodes attached to the NO pins on TS5A3359YZPR switches. I don't see them reflected on the datasheet but need some confirmation that they are present or not.
Thank you.
Part Number: TS5A3359 Other Parts Discussed in Thread: TMUX1511 Hi,
I'm designing low power device (powered from 4-20mA loop). I have 2x of TS5A3359, powered of +5V to GND rail. And two of these takes around 6mA current.
They are in static state:…
Part Number: TS5A3359 Good day,
Please can I be advised on whether the analog signal path (pins NO0, NO1, NO2, COM) is isolated from the digital control pins (pins IN1 and IN2)? If they are isolated is the GND pin then the reference for the analog signal…
Part Number: TS5A3359 Hello,
regarding the TS5A3359 analog mux, is there a "safest way" to have no-glitch on COM during power-up? E.g. assume the COM options should be passing either 5V, 3.3V or 0V (GND) to COM (depending on IN1 and IN2). So VCC…
Part Number: TS5A3359 Hi,
When we do not apply signals (IN1 and IN2) then what will be the default condition of below switch?
Please share your comments.
Thanks,
Kiranjit
Part Number: TS5A3359 Other Parts Discussed in Thread: TS5A3159 , Hi team,
I noticed that INO(pwroff) leakage current is much larger than INO(off) leakage current, why is that?
INO(off) means NO and COM is off, and the INO(pwroff) means ts3a3359 not power…
Part Number: TS5A3159 Other Parts Discussed in Thread: TS5A3359 , Hi team,
I want to confirm that if the TS5A3159 and TS5A3359 the IN control pin have internal pull-down resistance? I can not find detail about it in datasheet. Thanks.
Part Number: TS5A3359 Hi,
I found that TS5A3359 in my case can be right part for blowing MSP430 fuse, but have some questions.
In device absolute maximum ratings there is 6.5 VCC max, but it is not clear to me if device can switch 6.5V (Analog voltage…
Part Number: TS5A3359 Other Parts Discussed in Thread: INA190 , INA818 , ADS1115 , , LM2576 Hi TI Technical Support Team,
Recently, I have design and produced a PCB for battery charging and discharging. I am charging and discharging rechargable li-ion battery…
Part Number: TS5A3357 Other Parts Discussed in Thread: TS5A3359 Hi, We want to use this switch running at 5V power rail but controlled from MCU at 3.3V. Datasheet states that VIH is 0.7xV which for 5V gives 3.5V. Is this correct and does it mean it cannon…