The ADS5402 only have non-decimation and decimate by 2 mode. You will have to either change the sample rate of the ADC to be 76.8MSPS for non-decimation mode or 76.8MSPS*2 for 2x decimation mode.
For your learning experience, I would encourage to research…
User,
Consult the TRF3705 and LTC5585 data sheets regarding your LO input power question. As far as the GUI goes, the only documentation we can provide is from the TSW1266EVM User's Guide and the TSW3085EVM User's Guide, which can both be found on the…
Nikunj,
I would suggest you synchronize both clock generator's. You have a couple of options for providing synchronization. The TSW1266EVM allows for multiple clocking configurations by using the LMK04800 clock jitter cleaner and generation chip. A…
Sergio,
I would suggest you follow the TSW1266EVM User's Guide and get an output out of this board first. Do you have a TSW1400EVM or a TSW1405EVM to capture data from this board? If not, you can order one of these from the TI website. I would suggest…
Hi Jim
I found that TSW1400EVM can simplify my work together with TSW1266EVM
Can these two EVMs implement together ?
Further, the above link is now unavailable to download, can you provide the latest version of the firmware?
Best
Anthony
Girish,
I'm not sure I understand your question? The input signal goes through an IQ demodulator which does a complex down conversion to an IF signal, then I and Q paths are then sampled by the dual input ADS5402 ADC.
The output IF frequency is…
To whom who may concerns
After read through the source code of TSW1400, which is given by Jim Seton called "TSW1400_ADC_Firmware_12_12_14.zip",
I want to add some signal processing code (e.g. cross correlation) after the ADC(TSW1266EVM) data…
Hi,
I am using TSW1266EVM as broadband DPD, however I could not find any specification on demodulator being used. My question is, what is the maximum power which demodulator can handle without damage.
Thanks,
Meenakshi
Hi,
I am using following development kit for my system level design.
http://www.ti.com/ww/en/Altera/pg_dc.html
Can ti provide any initial demo FPGA programming file for using port A of FPGA to receive data from TSW1265 EVM?
Pin connections for HSMC-ADC…
Hi,I let my foreign friend buy tsw1265evm and tsw1266evm for me.I get the box today,but I only find the board and USB cable in every box. There are no power supplies in them.Ken.c had agreed to ship them to me.I had send address to Ken.c,but no one contact…