@The TCA9406/TXS0102 is not recommended when you have a cable with nontrivial capacitance, because too much ringing can make the edge accelerators trigger erroneously, and make it oscillate.
What do you mean by "too much ringing" ?
@With either…
These voltages imply that some other device sinks current. Is there anything else connected to these signal lines?
I do not know why that table mentions four-channel devices for UART. You could use the TXS0102 (which is like the LSF0102, but with edge…
Frank,
The SN74LVC1G3157 is a passive FET switch and will simply pass a signal from the drain to the source without any alteration. If you put a noisy signal on the input of this switch it will be noisy on the output. Garbage in garbage out kind of…
Other Parts Discussed in Thread: DRV2667 , TXS0102 I want to use the DRV2667 with my own MCU (which is not an MSP430). I am using a DRV2667-EVM to test my application, but I cannot figure out how to control the DRV2667 through I2C without the on-board…
I also want to know if I can use a 10K pull up resistor instead of what TI recommended 3.3K. Because the other side is TXS0102 Voltage-Level Translator, which low-level input voltage is only 0.15V max..
Part Number: P82B96 Other Parts Discussed in Thread: TXS0102 , PCA9515A , TCA9517A
Dear Technical Support Team,
I have two questions about P82B96.
I consider two cases for my connection.
Q1.)
I'd like to use two P82B96, but datasheet shows below…
I have been thinking about this and maybe in your case the serial resistors may not be a good idea. As an alternative I would suggest using a level translator like TXS0102, which would limit the output current in a short condition.
Hey Joe, Welcome to the E2E forums! For level translators, you would probably need a bidirectional translator from this page: www.ti.com/.../bidirectional-voltage-translation-products.page Our team supporting the LM25066 have not tested different I2C…