Part Number: UCC27712-Q1 Other Parts Discussed in Thread: UCC27712 , UCC25800 Tool/software:
I am trying to drive a motor high side using this driver as shown in the image. The Vsys is from 21-29V. I am only able to achieve 80% with motor connected and…
Part Number: UCC27712-Q1 Other Parts Discussed in Thread: UCC27712 , , UCC27211A-Q1 Tool/software: Hello team,
Good day!
Due to lack of IO source in MCU, customer need to combine HI and LI control by one signal with deadtime, if UCC27712 can support this…
Part Number: UCC27712-Q1 Dear Sir/Madam,
I am using Ucc27712-Q1 driver ic for driving my high and low side mosfet. Even after referring the Datasheet of the same i am unable to understand the turning off of High side mosfet.
Does low side mosfet places…
Part Number: UCC27712-Q1 Other Parts Discussed in Thread: UCC27712 , Tool/software: UCC27712.pdf
Hi TI team
I'd like to request the schematic review of UCC27712DRQ1.
The High bridge output 220V AC,the PWM freq is 50~60Hz.
1.For space save,is any part…
Part Number: UCC27712-Q1 Other Parts Discussed in Thread: UCC27714 , UCC27301A-Q1 , UCC21551-Q1 The lead-to-lead spacing between pins HS & LO in UCC27712-Q1 is 0.030 inches. we need 0.045 inches between those pins. Please suggest.
Part Number: UCC27712-Q1 I constructed the following circuit using two UCC27712QDRQ1 driver chips and four IRF150P221 n-channel MOSFETs. I stuck as close as possible to the reference design guidelines, although Cboot may be a bit larger than needed as…
Part Number: UCC27712-Q1 Other Parts Discussed in Thread: UCC27712
I am confused that its 10% to 90% parameter for Vgs or Vds in data sheet?
I use the tools to caculate the half bridge gate driver minimum current. The disired rise/fall time is the same…
Part Number: UCC27712-Q1 Dear TI experts,
My customer now tests UCC27712-Q1 with their own PCB.
But they have a problem with testing, so I want you to review the schematic first.
The schematic is confidential because it is still under developing.
so I…
Part Number: UCC27712-Q1 Other Parts Discussed in Thread: UCC27712 Hi Team,
I'd like to request the schematic review of UCC27712QDRQ1. It is used on three phase inverter application but the working of this device is abnormal. Please check the schematic…
Part Number: UCC27712-Q1 Hi,
Now we are using UCC27712-Q1 for motor driver (three phase).
Refer to the recommended layout as follow:
For three phase inverter application, three UCC27712-Q1 are used.
As the ground of MCU and the power of IGBT are common…