Other Parts Discussed in Thread: TPS65217 Hi guys !
So I've been trying to setup an environment development based on the BeagleBone Black, following the steps stated here . However, the rebooting of the board in the setup.sh fails after the uDev.txt…
Hello Tansel,
The UAF42 topology does not accommodate differential operation. I suggest using a multiple-feedback (MFB) active filter which lends itself nicely to a differential input, or fully differential filter. I wrote an article for TI's AAJ some…
Yes you can use the UCC28950 for primary side control withan opto coupler. You will just need to setup the voltage amplfier as a voltage follower by tying the COMP pin th EA-. You would then tie EA+ with a pull up resistor greater than 1K to Vref. Then…
Part Number: TDA4VM hi, expert,
i try to boot A core which kernel image residing in EMMC storage by modified boot_app_mcu_rtos(ti-processor-sdk-rtos-j721e-evm-07_03_00_07\mcusw\mcuss_demos\boot_app_mcu_rtos), but it failed, the boot process log is like…
I wrongly clicked "This solved my issue". Sorry!
Bryan Lizon86 said: Regarding the M pins: since I cannot see the bottom of your board, this means you have soldered on resistors to the correct locations to tie these pins to their respective levels?…
Hi
From the log message: Modules linked in: ... [last unloaded: bc_example],
I traced the all loaded modules in system by lsmod command, observed that the "bc_example" module on the list.
then unload the module by rmmod command,
We couldn't unload…
Hi Keerthy,
Sorry for the delay in response. After reducing the Data rate for 1333MT/s our board crash started after 3Hrs. but still we are able to see the crash in the code. we had a discussion with your team to update the EMIF sheet for 1600MT/s.…
I tried kemal, didn't work. So i just changed and tried.
Please see the kernel log belwo:
U-Boot SPL 2017.01-00444-g17f04de-dirty (Feb 20 2018 - 11:44:24)
DRA752-GP ES2.0
Trying to boot from MMC2_2
*** Warning - bad CRC, using default environment…
Do you have the following config set?
CONFIG_AM335X_CONTROL_USB=y
CONFIG_AM335X_PHY_USB=y
CONFIG_NOP_USB_XCEIV=y
Attached below is my .config for v3.12.17 which works with g_serial.ko.
_config.v3.12.17-musb-builtin.txt
root@am335x-evm:~#…
Part Number: TDA4VM
Hi,TI
Now we found Serror on our TDA4VM board when driverring WIFI module in PCIE0. The error log as follows:
Starting kernel ...
failed to set vqmmc-voltage to 3.3V
failed to set vqmmc-voltage to 3.3V
[ 0.000000] Booting…